Product FAQcopterquadcopterflyhelicopterprofessionmotorkitmini

[FAQ]Anonymous asked about Crazyflie Nano Quadcopter Kit 10-DOF with Crazyradio (BC-CFK-02-B)

I just want to ask if it would be possible to add a gps sensor to the board or something like that to fly it gps controlled? It also would be interesting to know if such signals (gps or maybe a camera signal) can be transferred via the 2,4GHz radio str
https://www.seeedstudio.com/Crazyflie-Nano-Quadcopter-Kit--10-DOF-with-Crazyradio-(BC-CFK-02-B)-p-1365.html

Patrick EuerleOct 19,2016 20:16 PMAdd Comment

Comment

Popular Topics