grovebeaglebonegrovelinkit

[Awesome Projects] Grove Environmental Sensors

Here is a collectionofprojects using Grove environmental sensors. It is the most popular Grove category so far.The idea is to share development tools(even  with same project ideas) and creative applications. If you want to share your own, feel free to comment below. In most cases, these tutorials can be used in various sensors specially when the protocols are the same. Here are some key words for you to better navigate the projects.

[Board]
Raspberry Pi, ESP8266, Intel Galileo/Edison,Light Blue Bean,Arduino UNO, Seeeduino UNO

[Cloud]
temboo,twilio,Windows 10 core,initial state, Mediatek Cloud Sandbox,Intel IoT Analytics Dashboard,

[Libraries]
Johnny Five, upm(MRAA)


1.Barometer Sensor

bluetooth low energy (BLE) weather station by Vincent Dupuis
abluetooth low energy (BLE) weather station with its associated smartphone (in my case iphone) app.


Build a Weather Station By MediaTek Linkit ONEbystatusorel.ru
Upload data to internet and streamed on the cloud via Mediatek Cloud Sandbox


2.Moisture Sensor


upm:  GroveMoisture Class Reference
API for the Grove Moisture Sensor by using the MRAA libraries


Making a plant watering reminder system with LaunchPad & Energia!byAdrianFer,TI
Reading the analog Moisture sensor and triggering a text message with Temboo & Twilio.


Water Detection System by Karel Kalthoff
Send email alerts with LightBlue Bean using Node-RED on Raspberry Pi


Intel Edison Hydroponics Controller by  BLT Robotics
Creating a IoT enabled Hydroponics Controller using the Intel Edison, Intel's XDK IoT Edition, which allows you to write your code in JavaScript using Node.js libraries, as well as Intel IoT Analytics Dashboard.


An Introduction to IoT with Arduino, Node and a Plant by Leonardo Couto
runningjohnnyfiveonarduino,light up a LED, print something on LCD and read data from moisture sensor even make a twitter bot for the plant


3.Temp& Humiditysensor


Review: Wio Link Plug-and-Play IoT Board by initial state team
use Wio Link to stream data of temp&hum sensor to Initial State with IFTTT and with Python.


4.Dust Sensor

Indoor Air Quality Monitoring by Bo Wang
detect the particle pollution emitted by cooking activities to investigate correlation of cooking behaviors and air quality wiithArduinoUno Ethernet. It reads the data from the sensor and writes to serial port of the computer.


Air Quality Box by Seeed Studio
Monitor air quality around you with data of alchoho sensor, gas sensor, dust sensor on OLED display over Seeeduino UNO


5.Air Quality Sensor


Intel Edison + Grove - Air quality sensor byrwaldron
Using Johnny-Five with Grove's Air quality sensor component on the Intel Edison Arduino Breakout. This shield and component will work with any Arduino pin-out compatible hardware platform.More  Johnny-Five on Intel Edison + Grove IoT Kit Examplesdison + Grove IoT Kit Examples


ESP8266 and Air Quality sensorby fab-lab.eu
ESP8266 hooked up to the cloud feeding data from an Air Quality sensor sniffing for  VOCs (volatile organic compounds) are emitted by bread... with astonishing results!


[WEARABLES] LEAIRF: AIR QUALITY DETECTION NECKLACE by Jiashan Wu
A wearable necklace indoor air quality detector with a mobile display app.


6.Gas Sensor


A Plant Box with Lightning and Rainingbyloovee in Seeed Studio
use  Raspberry Pi 2 running on Windows 10 IoforT Core to collectdata outdoors such as temperature, humidity, and CO2 to a plantbox


Python on Intel Galileo/Edison – Part6: Light sensor by NavinBhaskar
usingtheupm library to interface the Grove Light sensor with the Galileo/Edisonusing python.


Home Automation: Control Relay Base On Light Sensor (Intel Edison) by Nghia Nguyen
Every night before go to bed, you always have to turn on the alarm system.


7.Sound Sensor


Intel Edison and Grove sound sensor - Send message to mobile via MQTTbyGlaucoJ


8.Light Sensor


Example: Light Sensor by Paul Langdon
Sample Light Sensor on Intel Edison in Node.js

BerlinaJul 26,2016 07:45 AMAdd Comment

Comment

Popular Topics